Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Workflow: Interface for the user

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

you may add it only into the instruction filed of the perform signoff task.

Michael
Teamcenter UA | NX CAD

Re: Workflow: Interface for the user

Gears Phenom Gears Phenom
Gears Phenom

Hmm... do Workflow tasks have stylesheet?

Re: Workflow: Interface for the user

Gears Phenom Gears Phenom
Gears Phenom

I think this can be done using customization:

 

Customize the workflow signoff pane

https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help#uid:xid1256877:index_programmers_guide:i...

Re: Workflow: Interface for the user

Phenom
Phenom
Yes, epmtask has a stylesheet. I modify the tables that show reference and target objects to include properties that users should have set e.g. material and finish, also other mandatory fields. I think the stylesheet applies to all tasks, but you could change the display based on the type of task I think, or you could register a new stylesheet I guess.
Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: Workflow: Interface for the user

Pioneer
Pioneer

@Michael_Ruhnke

Yes sure but it takes time when you've a lot of workflow.

 

@ArthurRM
Yes I found the stylesheet. I need to test tomorrow. And thank you for the documentation

 

@ProspectPLM

Thank you for your answer. I will work on that

PLM Consultant / Switzerland

Re: Workflow: Interface for the user

Phenom
Phenom

Stylesheet for task is BaseEPMTaskSummary:
Capture.JPG

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: Workflow: Interface for the user

Pioneer
Pioneer

After some analyse, my idea is to try to develop the customisation as it is suggest by one of you in the case.

 

If it's a success in some weeks, I will give to you an input.

 

Thank you for all of you about your support.

PLM Consultant / Switzerland

Re: Workflow: Interface for the user

Phenom
Phenom

I havent tried this but its worth a try.

 

Updated the 'Display Name' business constant on the EPMTask/EPMJob in BMIDE to include Root Task Template name.

This usually works for all business objects.

 

Mahendra