Cancel
Showing results for 
Search instead for 
Did you mean: 

Workflow: Modify a PRT (UGMASTER or UGPART) when a status is present

Valued Contributor
Valued Contributor

Hi everybody,

 

I create a workflow to can be Troubleshoot a drawing when he have a status of protection.

 

To do that, I use an ACL and the handler (EPM-set-rule-based-protection) to open the Revision (Works for the stylesheet). But I cannot save the drawing.

 

I think it's because the drawing have some links but if I remove the status, I can edit without problem.

 

I try to explain as better I can but have you a solution ?


Thank you

 

 

2017-11-23_17h32_37.png2017-11-23_17h33_16.png2017-11-23_17h34_04.png

PLM Technical IT