Cancel
Showing results for 
Search instead for 
Did you mean: 

WorkspaceObject : Save - PreCondition ? Operation, Extenstion, Property Condition ?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello Experts,

 

We have a WorkspaceObject and having 2 attributes on it.

AttrA = Boolean

AttrB= String

 

We have a requirement that if the AttrA is set to true, AttrB should be Filled/Required.

I checked BMIDE but their is no Operation available on WorkspaceObject to have a Save PreCondition.

 

Request you to please suggest some Ideas how this can be achieved.

 

TC Version: 11.4.03

 

2 REPLIES 2

Re: WorkspaceObject : Save - PreCondition ? Operation, Extenstion, Property Condition ?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
What kind of WSO? Everything is not possible without code.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: WorkspaceObject : Save - PreCondition ? Operation, Extenstion, Property Condition ?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

It is Just a child Type of WSO, It is perfectly fine to customize as we do not have any option in the RAC Rendering to have Conditional property. PreCondition on Save of WSO

For example we can take Folder, 2 Attributes

But the Problem is we do not have any save Operation on it ...

 

requirement is if the AttrA is set to true, AttrB should be Filled/Required.

 

FolderWSO.png