Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

any suggestion on when to create a new volume in teamcenter?

Genius
Genius

any suggestion on when to create a new volume in teamcenter?

3 REPLIES 3

Re: any suggestion on when to create a new volume in teamcenter?

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon,
You can create a new volume in the Organization application:

new volume.png

To correctly fill in the required fields, you can use the existing volume as a basis.

Re: any suggestion on when to create a new volume in teamcenter?

Legend
Legend

You would typically create new volume if volume contains so many files/directories that volume operations become slow or you start coming close to the OS limit on inodes.

 

Keep in mind that, if you create new volume and move users over to new volume, you will see that # of files in the old volume will start to go down over period of time. This is becuase, as users release datasets, purging action will start to delete older files from volume and you will see that older volume start to shrink again.

---

Thanks and Regards

Yogesh Fegade

Re: any suggestion on when to create a new volume in teamcenter?

Legend
Legend

OR, obviously, when drive/disk containing volume fills up :-)

---

Thanks and Regards

Yogesh Fegade