Cancel
Showing results for 
Search instead for 
Did you mean: 

attach dataset automatically to item rev

Pioneer
Pioneer

Hi experts ,

I have requirement ,that

when i create a item  , the dataset should be attched with item rev automatically.

I tried in BMIDE using operations , but it is attaching with item .

 

Thanks.

4 REPLIES

Re: attach dataset automatically to item rev

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Not so easy to figure out what is going wrong with the information you provided but if you define a postaction on the revision on ITEM_create_rev the dataset must be attached to the revision and not the item.

xtof

Re: attach dataset automatically to item rev

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Girish posted the question in both the User and Admin forums. I'm only going to answer in this forum. The solution is IRDC. It's designed to add a Dataset to the Item Revision when the Item is created. IRDC is configured using BMIDE and you can find good examples in the documentation.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: attach dataset automatically to item rev

Siemens Creator Siemens Creator
Siemens Creator

You can use IRDC to set up templates where any kind of dataset can be attached on creation. 

Re: attach dataset automatically to item rev

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello,

 

You may want to try setting up 'automateAndLink' extension to 'Create(Teamcenter::CreateInput*)' operation post-action on your Item.

 

Arguments for this extensionRule will be:

TargetObjectType: <select the dataset object>

RelationName: <select the relation name>

RelationHint: SourceRevToTargetRev

 

Harish