Cancel
Showing results for 
Search instead for 
Did you mean: 

cancel checkout from NX menu (ANT)

Builder
Builder

We have intrudced rule for TC+NX users that they need to checkout the part if they want to edit the changed and check-in to commit the changes

 

So from NX they can

  • Check IN
  • Check out

 

NX_Save.PNG

 

 

From Teamcenter 

  • check in
  • Checkout
  • Cancel Checkout

checkout.PNG

 

 

 

if users majorly work with NX (Launching NX in integrated mode without RAC), there is  no option for "Cancel Checkout"??

 

Please advice

 

3 REPLIES 3

Re: cancel checkout from NX menu (ANT)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @nesthome,

In customer defaults settings, there are four options available for check out/check in policy. You can set it as per the requirement.

TCNX_CICO.jpg

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: cancel checkout from NX menu (ANT)

Builder
Builder

@ 

 

yes we are using that option, but once there checocut in While they are in NX, there no way to cancel the checout.

 

  1. user open the model, as readonly
  2. if he want to edit, he will manually checout in NX ANT
  3. Now after checking out, he decided he doesnt want to commit checkin
  4. he want to cancekl the checkout, As of now there is noway he can CANCEL Checkout  from NX navigator

Re: cancel checkout from NX menu (ANT)

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

So if you are thinking that you will need to extend the functionaility of NX managed. You can create your own blockstyler menu button. 

 

You'll have to get:

1) a teamcenter session connection

2) the Model Object that you want to cancel check out

3) the reservation service in SOA has the cancel checkout functionality.

 

resService = Teamcenter.Services.Strong.Core.ReservationService.getService(TCSession.GetConnection());