Cancel
Showing results for 
Search instead for 
Did you mean: 

change TcServer Character Encoding Settings manually

Genius
Genius

Hello;

I want to change/check "TcServer Character Encoding Settings" after installing client. Is there anyway to do that?

when I use RapidStart then PreConfigured installation choice, there is no step to change this setting in installation.

 

I really appreciate your hepls.

Best Regards.

1 REPLY 1

Re: change TcServer Character Encoding Settings manually

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon,
I'm not entirely sure, but it looks like the value of the encoding during the installation is recorded
in TC_DATA\tc_profilevars.bat line:
set TC_XML_ENCODING=windows-1251

You can try changing it, if you have 4 Tier, do not forget to restart Teamcenter Server Manager