Cancel
Showing results for 
Search instead for 
Did you mean: 

checkForSave on custom java form

Valued Contributor
Valued Contributor

Has anyone been able to get "checkForSave()" to actually work on a custom Java form? CheckForSave() is a function on the AbstractRendering object that I'm extending for my form. 

 

I'm using a custom java form to create an ECO form and if someone clicks on another object while editing the form they lose all their changes without a warning. The checkForSave function is suppose to be able to run custom code when someone selects a new object but it seems to never fire.

 

I'm working in TC 8.3.3 but I'm curious if anyone has been able to get this to work in any TC version.

1 REPLY
Highlighted

Re: checkForSave on custom java form

Valued Contributor
Valued Contributor

I talked with GTAC and they said I need to add the below function. This works for me!

public boolean isRenderingModified(){

   logical isModified = true;

   //add custom code here to determine if form is modified

  return isModified;

}

 

checkForSave() doesn't seem to do anything. The 8.3 documentation is wrong.