Cancel
Showing results for 
Search instead for 
Did you mean: 

classification systems

Genius
Genius

Hello;

I have a specific need related to classification system.

I have 2 different classification systems and I want:

1. create a link between these 2 classification systems

2. classify an item in both of the classification systems(connect an item to 2 classes)

 

Anyone can give me any idea?

I really appreciate your help.

BR

2 REPLIES 2

Re: classification systems

Genius
Genius

No idea for classifying an item in 2 classification system?

Re: classification systems

Siemens Genius Siemens Genius
Siemens Genius

I am not sure what you mean with "Classification Systems" in Teamcenter Classification.

But it is possible to classify one item into multiple classes.

It is also possible to classify the same item multiple times in the same class.

(In that case you have to enable it in Classification Admin for this class. (Allow multiple instances))

 

You can find info also in the TDoc:

Classifying Data - Classification - Working with classification objects

Classifying an object multiple times

 

Hope this helps...

 

   Markus