Cancel
Showing results for 
Search instead for 
Did you mean: 

custom relation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

hi

I create a couple of custom relation for the revision, then i display them as a pseudo-folders.

Is it possible to change the icon for particular relation. i can't find info in the manual

 

 

--
regards
dj
2 REPLIES

Re: custom relation

Creator
Creator

The custom relation pseudo folders have standard icon type. I guess one cant change it. I am using TC9.1 i haven't seen any option for that.

 

chini

Re: custom relation

Pioneer
Pioneer
You might be able to set up a property renderer on the PseudoFolder object.
But I never tried on PseudoFolder objects.
Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP4 + TC10.1.7.1
Testing: NX11.0.2.7 MP4 + TC10.1.7.1
Development: C#