Cancel
Showing results for 
Search instead for 
Did you mean: 

decimal point definition

Creator
Creator

hi,

 

we have a new requirement to store measurements in teamcneter with 4 decimal places.

 

Storing it as a string is not not good enough, as the number is going to be derived using calculations run during a workflow. All display of the attribute MUST be in 4 decimanl places within Teamcenter.

 

This may sound like a "really" simple question, but is the correct way to approach this to use a Naming rule on a Double based attribute? I'm just curious to know if there is a more elegant way of doing this than using a naming rule.

 

Thanks,

2 REPLIES

Re: decimal point definition

Genius
Genius

see GTAC PR - 8885265

Re: decimal point definition

Creator
Creator

thanks for your reposnse.

 

However, at 10.1.6.1, the "fnd0DecimalDigits" property constant is unavailable.

I will, in the meantime, see if teh default of 4 decimal places will work (according to the PR).