Cancel
Showing results for 
Search instead for 
Did you mean: 

disable Create JT button in Save manager of Catia integration with TC

Builder
Builder

Hello,

 

Is there a way to disable Create JT button in catia integartion. We can hide it through the savemanger.xml. But when that button is turned on before the hide, it still generate blank JT.  Below: where is the com.ebsolutions class? Will it help is I delete the ****actions.CreateJTaction? Thanks everyone111111111111111111.png

3 REPLIES

Re: disable Create JT button in Save manager of Catia integration with TC

Genius
Genius

CATIA_createJT_option is preference which control enable and disable of JT button in Savemanager.

Now this preference is get instantiated on user level also whenever User perform any Save Action.

 

So you have to remove all instances of this preference from User level first and then set the preference with value false at site level and then you can remove the button definition from SaveManager.xml

Re: disable Create JT button in Save manager of Catia integration with TC

Builder
Builder

Thanks for the reply. I do think this is the easiest way. I just don't understand why the button is still active after we hide the definition in XML...

Re: disable Create JT button in Save manager of Catia integration with TC

Genius
Genius

This is because button is hide in Panel but it is not disable.

Enabling/Disabling mechanism here driven by preference which is get instatitaed at Site/User level also.