Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

installing another tc server for LB

Pioneer
Pioneer

Hello;

I need to install another tc server for LoadBalancing.

Shall I copy the tcdata folder from the current server to the new one and choose "Use populated database and existing data directory" option?

 

Thanks.

BR.

1 REPLY 1

Re: installing another tc server for LB

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You do not need to copy TC_DATA to another location, simply "share" it and use the UNC path. Use populated and use existing then point to the existing TC_DATA.

However, server manager doesn't really do load balancing, it just selects the next available from A then B then A, etc. It does better at fail over than load balancing. For LB, consider multiple web tiers behind an F5.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4