Cancel
Showing results for 
Search instead for 
Did you mean: 

issue logging into management console

Valued Contributor
Valued Contributor

Hello;

I have installed managemet console, but when I try to log into it first time using admin/admin I get an error "the login attemp failed". Anyone can help?

the log is this "security failure during user 'admin' authentication: Failed to complete authentication process due to the following error(s) ERR_04201 No more characters availavle at position 24"

I use TC 11.4.0.3 with Java 8u45

 

Thanks.

BR.

2 REPLIES

Re: issue logging into management console

Legend
Legend

What do you use as webserver?

Have you followed all the steps in the "Install Teamcenter Management Console" and did you select embedded ldap or external during the setup?

 

I use embedded ldap and configured TomCat where I adjusted the catalina.bat file.

restarted and all worked fine.

This setup is alot better than the previous webtier console I used for TC10.x togheter with .NET.

 

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018

Re: issue logging into management console

Valued Contributor
Valued Contributor

Thanks Jormh.

I think it was ldap issue I changed it to internal and then it worked.

 

Br.