Cancel
Showing results for 
Search instead for 
Did you mean: 

issue to open a xml file in a Text dataset

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everybody,

 

I'm meeting an issue to open a xml file which is in a Text Dataset.

That is the message i have:

2018-04-06_11h25_11.png

 

Do you have any idea ?

9 REPLIES

Re: issue to open a xml file in a Text dataset

Phenom
Phenom

Hello, are you trying to open it with a double click in a separate application or in the built-in viewer?

Re: issue to open a xml file in a Text dataset

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Thank you for your quick answer.

I can see the xml in the built-in viewer but not with a double click.

 

Regards.

Re: issue to open a xml file in a Text dataset

Phenom
Phenom

I checked it myself, it seems I do not have these problems, write your version of the viewer. Your JT files are normally displayed in the built-in viewer?

xml in text ds.png

Re: issue to open a xml file in a Text dataset

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Artur3,

 

I can see my XML in the viewer Smiley Happy

 

It's when I do a double click that I have the issue.

 

Regards,

Re: issue to open a xml file in a Text dataset

Phenom
Phenom

Yes, I'm sorry, I misread your answer.
What is the associated * .xml on your computer? And what version of IE do you have?

Re: issue to open a xml file in a Text dataset

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

I'm using IE 11 and the program to open xml in my computer is notepad++

 

Sorry but I'm not sure to anderstand when you said :"What is the associated *.xml on your computer?"

Do you want the tool to open xml (notepad++) or the xml itself ?

 

Regards

Re: issue to open a xml file in a Text dataset

Legend
Legend

I think he wants to know the program associated with the file extension:

file_association.JPGRichard

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: issue to open a xml file in a Text dataset

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

OK, so in this case, the program associated is Notepad++

 

Regards,

Re: issue to open a xml file in a Text dataset

Phenom
Phenom

Antispam removes my answer...

 

Good afternoon, I also use Notepad++

As it turned out to be a simple change in the association of files, the problem is not solved, it is necessary to make changes to the registry.

1) Do an association of xml files with Notepad++

2) Make changes to the registry

Works for me (I have Windows 8.1 and IE10):
For IE10 the Windows registry modification should be as follows: HKEY_CLASSES_ROOT\XEV.GenericApp\shell\open\command Defaults from "C:\Program Files\Internet Explorer\iexplore.exe" %1 To "C:\Program Files\Notepad++\notepad++.exe" "%1"

For IE11 the Windows registry modification should be as follows: HKEY_CLASSES_ROOT>xmlfile>shell>open>command Defaults from "C:\Program Files\Internet Explorer\IEXPLORE.EXE" %1 To "C:\Program Files\Notepad++\notepad++.exe" "%1"

I did not test the changes for IE11; I have it not installed.

Before changing the registry branch, make its export (backup) so that it can be returned to its original state.

Your installation paths for Notepad++ may differ, I tested on the x64 bit version of Notepad++, I do not work with x86.