Cancel
Showing results for 
Search instead for 
Did you mean: 

kinematic dataset on item Creation setup in BMIDE

Creator
Creator

Hi experts!

 

As a new guy using BMIDE I'm in need of help understanding how I can create a kinematic dataset on the item revision level automatically when creating a item in Teamcenter (custom business item that i created in BMIDE). This custom business object is supposed to work as a compoundobject in Process simulate and should be able to be opened for modeling/end modeling. 

 

As i understand it I should be able to use the IMAN_save operation in the operation tab of the Custom object. By adding the extension createObjects on PostAction here I should  be able to select the arguments for KinematicRelations. 

 

However when browsing Extension (operation tab for the itemrevision of my custom object) i cannot select createObjects. Only Fnd0ValidationSavePost, automateAndLink, Fnd0TcifPostSave. 

 

I checked the availability on createObjects extension (extension folder) and i do not have the IMAN_save operation present on Item, ItemRevision. Nor can I add or edit the availability list. 

 

What i would like some help with is:

 

1) Am I thinking correctly regarding of how to create a automatic dataset on item creation in TC for my custom object?

 

2) If I am. how do I go about to add IMAN_save on the extension createObject?

 

P.S. If I am totally wrong i would love some help with some sort of guidance of how to setup the business object in BMIDE for creating a kinematic dataset on the itemrevision level in TC.

 

 

2 REPLIES 2

Re: kinematic dataset on item Creation setup in BMIDE

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
In my Tc11.3 environment, I see createObjects available under ITEM_create_rev/PostAction.
Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: kinematic dataset on item Creation setup in BMIDE

Creator
Creator

I figured something might be different since i do not have it as an option and secondly I can not add/change in the availability list for createObjects extension. 

 

Im guessing that if that was possible to add createObjects on ItemRevision i would be able to achieve what I was trying. 

 

Any suggestions of why  the extension createObjects is uneditable in my environment?