Cancel
Showing results for 
Search instead for 
Did you mean: 

mapping NX 12 and TC11.6

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi

I am trying to get the calculated weight in NX (NX_Mass) over to a TC attribute on a custom itemtype revision.

I did set the preference "TC_NX_allow_attrsync_master_iman" to "yes"

And added the rows before for "SV4Design" which is my new item type...However it simply does not synch the weight from NX...So any ideas?? I have looked over spelling a couple of times..but are there obvious wrongs in the syntax?? Or can weight not be synched like this anymore??

The attribute I synch to is a string attribute...does it need be "Double" or "Integer" perhaps??

 all responses much appreciated...

 

}

{ Dataset type="UGMASTER"
    "DB_PART_NAME" : Item.object_name /write_once /description="Part Name"
    "DB_PART_DESC" : Item.object_desc /write_once /description="Part Description"

    { Item type="SV4Design"
        NX_Mass : ItemRevision.sv4_TotalWeight /master=both /description="Total Weight"
    }

}

2 REPLIES 2

Re: mapping NX 12 and TC11.6

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, yes, your attribute should be of type Double, I don’t see any errors in the syntax of the NX_Mass attribute, I would just do /master=cad

Re: mapping NX 12 and TC11.6

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
thanks that did the trick...