Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

nx8.5 within teamcenter 8.3 run and many tab is not show?

Pioneer
Pioneer

Dear Friends


In native NX8.5 when we open the software, in the new dialog box we see many tabs like Modeling, Drawing, Simulation, Manufacturing, Inspection, Mechatronics Concept Designer and Ship Structure. But when we want to create the new part in NX8.5 from within Teamcenter8.3 we will only see the Modeling, Manufacturing and simulation tabs. For example it is not possible to create drawings using the master model workflow. How can we fix it?I need to have Drawing Tab.

 

thanks

7 REPLIES 7

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Search the NX documentation for UGII_TEMPLATE_DIR, which is the folder containing the PAX files, that are used to specify the tabs in the file new dialog.

 

Spend some time reading the information provided in the NX help file about the file new template pax files.

In addition read through the NX integration for Teamcenter section of the NX help file.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Pioneer
Pioneer

can tell me more information about this? and how to solve it?

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Valued Contributor
Valued Contributor
Dig into your Syslog file.
Search for "pax" and you will be told why and which entries of your configuration were discarded.
Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP04 + TC10.1.7.1
Testing: NX12.0.2.9 MP07 + TC12.1.0.2
Unstable: NX1847
Development: C#

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The documentation can be found in the NX help file under the topic Fundamentals => Working with files (or Managing files) => Part file templates.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

While both native and managed NX look at the same directory, they don't load the same templates (pax). Native NX loads ugs_*.pax while managed NX loads nxdm_*.pax. The OOTB directory where templates are stored is %UGII_BASE_DIR%\UGII\templates. There is a "sample" subdirectory that contains "tcin_template_setup.bat" which basically looks for files beginning with nxdm in "templates" and tries to copy them to "sample". Make sure to delete existing "sample\nxdm*.pax" before running the script. Read the script lines 349 - 362 for an explanation.

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Experimenter
Experimenter

A few Points to note

 

PAX  Files

 

In Teamcenter Env, these can be stored inside the Teamcenter Database.

For NX8.5, 

TC_NX_FileNewPAXFiles_NX85 is the Teamcenter Preference, which contains the ItemRevision which contains the text dataset, which has the PAX file contents.

 

In General, the Preference is TC_NX_FileNewPAXFiles_NX?  ( ? is the NX Version ).

This can be set as a Teamcenter Group Pref also.

The Pax file, contain, details of the Template, etc.

 

I am attaching 2 GTAC articles, which will help you.

 

Hopw this helps.

 

 

 

 

PLM Consultant

Re: nx8.5 within teamcenter 8.3 run and many tab is not show?

Excellent answer, I left out the 5 in the preference and didn't realize it until I read this post. THANK YOU!