Cancel
Showing results for 
Search instead for 
Did you mean: 

problem with ITK "link_custom_exists"

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Hi,
 
I have a problem with ITK. I created a custum handler and I want to test it. but here is the problem. I can compile the code but when i want to create the dll with the batch file "link_custom_exists" I have an error saying:
"mt.exe : general error c10100b1: Failed to load file "liba3mylib.dll". The system cannot find the file specified."
"liba3mylib.dll" is the name of the library i created in the BMIDE.
 

And among the files generated, there is no dll file.

 

Can someone help me please?

 

Thank you.

 

Regards,

 
 
1 REPLY

Re: problem with ITK "link_custom_exists"

Phenom
Phenom

As per the doc, you need to package the BMIDE template and the package will contain the libraries.

 

https://docs.plm.automation.siemens.com/tdoc/tc/11.3/help#uid:xid1256815:index_plm00071:id443832:xid...

 

 

The Business Modeler IDE packages the built C++ library as part of its template packaging. The complete solution that includes the data model and the C++ run-time libraries are packaged together.