Cancel
Showing results for 
Search instead for 
Did you mean: 

ps_upload Utility

Experimenter
Experimenter

Hi All,

 

  Items from the text file not created while running ps_upload utility

 

 Running ps_upload utility from teamcenter command prompt

 

Teamcenter Version

 

Tc10.1.0

 

Text file :

 

#DELIMITER >
#COL item name level seq type rev
000016>Fastern Categories>0>->S9_Screw>A
000017>Wood Screws>1>10>S9_Screw>A
000018>Machine Screws>1>20>S9_Screw>A

 

Syntax: 

 

........TC_BIN>ps_upload –u=infodba –p=infodba –g=dba  –c=Item  –i=file path

 

Input From Standard Input<stdin>  // stopped working after this line

 

 

Please suggest

3 REPLIES 3

Re: ps_upload Utility

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

Change your delimiter to something that batch scripting won't get confused by. The tilde (~) is a good choice but still may be used in a description someplace and parse where you don't expect it. Some utils except double chars as a delimiter and the usage of ~~ is not normal in a description. Check if you can double the delimiter for better results.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: ps_upload Utility

Creator
Creator

Hello all,

 

will auto assign items ID's can be possible using ps_upload utility?

Re: ps_upload Utility

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Not that I know of.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4