Cancel
Showing results for 
Search instead for 
Did you mean: 

redeploy template without incorporating Latest Live Update Changes

Genius
Genius

Hi,

I just updated from TC11.2.1 to 11.3

Update finished successfully, but now I can not redeploy our custom template

There were live updates deployed before the Update and now it's not possible to redeploy custom template anymore

It is also not possible to incorporate latest live updates into the template, BMIDE tells me there is no difference

Is it possible to force a tem update of the template?

I know, that all live updates are in the template, which I want to redeploy.

 

Thanks

2 REPLIES

Re: redeploy template without incorporating Latest Live Update Changes

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Did you do "Re-tun Template Project Upgrade Wizard" ? This will update it to latest data model and then there will be differences.

Re: redeploy template without incorporating Latest Live Update Changes

Genius
Genius

Hi,

I tried "Re-tun Template Project Upgrade Wizard" and a few more things, but I was not able to change the template, so it 'Incorporated Latest Live Updates' successfulls.

At the end, I connected directly to the Database, and was able to force the redeployment.

I did not want to restore the Backup, since the Update itself was successful.

 

Now it's running on 11.3 and full deployment works.