Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

set user friendly error message in a workflow

Creator
Creator

Hi. I have built a workflow with a condition task in it and I want the user to get a message if the condition goes along the F path. The designers at this company never used the workflow viewer and the best thing would be some kind of pop-up message. is this possible without entering the workflow viewer? 

 

I've tried using the handler EPM-run-external-command with -lov as argument and "INPUT~ErrorMsg1="message"".

this handler however will not give me a message until i enter the workflow viewer