Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

set user friendly error message in workflow

Builder
Builder

Hello all,

 

When using EPM-check-object-property handler, the popup error message is usually not very user friendly. For the first time user, it is hard for them to start the workflow since we plan to put it at START stage of START. If they are not all filled out, the workflow won't be started. 

 

So my question is where and how can I set that error message, like "please fill out all the properties listed below to start this workflow".

 

Thanks

6 REPLIES 6

Re: set user friendly error message in workflow

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Check out the presentation from Brian Horne - Workflow Design Best Practices...

http://www.plmworld.org/p/do/sd/topic=1032&sid=7350

Slide 14 talks about adding "Instructions".

 


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: set user friendly error message in workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

I usually do not add such rule handlers to the start action and instead add them to a separate Validation Task where the error path takes the user to either a Do Task with a better error name and instructions or a generic Task where I add a notify mail handler to send the user a detailed email with reason for the error and instructions to fix the problem.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: set user friendly error message in workflow

Builder
Builder

Hello Larry,

 

Thanks for the advice. I followed your advice. Came up with the workflow like this. 

 

One problem I had is where should the "fill in missing attr" task output go to? I am assuming it will be a closed loop until all the properties are good. 

The path in the figure between validation task and the task seems not work well.

Thank you very much 

Re: set user friendly error message in workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

You'd want a 'Do Task' instead so that the user see it in their inbox.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: set user friendly error message in workflow

Builder
Builder

OK. Thanks, I will try that

Re: set user friendly error message in workflow

Valued Contributor
Valued Contributor

Hi,

 

you can customize XMLs under %TC_ROOT%-->lang --> textserver-->en_US folder.