Cancel
Showing results for 
Search instead for 
Did you mean: 

target "-clean" command in Teamcenter start link

Valued Contributor
Valued Contributor

Hi everyone,

 

I found the follwoing start command for Teamcenter: "-clean".

 

Does anyone of you know about this command? I only know it will clear the cache where the start screen is located....but any other cached files???

 

any idea appreciated Smiley Happy

 

br

Jul1an

 

 

2017-02-02_15h02_27.png

 

 

4 REPLIES

Re: target "-clean" command in Teamcenter start link

Genius
Genius

Cleans cached data used by the OSGi framework and Eclipse run time. This is useful if you have new plug-ins you have added to your environment. It helps to troubleshoot startup errors after installation, update, or using a shared configuration.

 

Regards

Naveen Gowda

TC11

Re: target "-clean" command in Teamcenter start link

Valued Contributor
Valued Contributor

Hi naveengm,

 

do you see any issue if we constantly use this parameter in our start links?

br

Jul1an

Re: target "-clean" command in Teamcenter start link

Legend
Legend

There shouldn't be any issue in using clean option everytime.

But time taken to launch the RAC UI will be slightly more when compared with launching the RAC without clean option

 

Regards

Mahendra

Re: target "-clean" command in Teamcenter start link

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I disagree. Using the "-clean" option will remove any settings the user has made like "do not show this dialog again" or their column settings. The "-clean" option should be only be used occasionally, if at all. It's easier to just delete the folder instead of configuring the "-clean" option. At least you have more control over when the cache is deleted.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2