Cancel
Showing results for 
Search instead for 
Did you mean: 

two Pool managers not working parallely

Legend
Legend

Hello Team,

 

We are using Linux OS for Teamcenter Server, Where we have two Pool Managers, 

One for SSO and one for non-SSO, 

When I am starting both Pool Managers only the pool which started first is working.

I have used separate ports for both the pools,

What may be the reason for not working parallelly?

 

Regards,

Ganesh

2 REPLIES

Re: two Pool managers not working parallely

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Did you use unique pool id's? For example, SSO is TcPoolA and Non-SSO is TcPoolB. As long as the pool managers are on separate servers then the port number can be identical. They only have to be different if they are installed on the same server. However, the Pool ID must be unique for each set of tcservers.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: two Pool managers not working parallely

Legend
Legend

Sorry @RandyEllsworth for late reply,

 

Actually Pool ID's are different, still only one pool is running,

We are checking by increasing the RAM size as it was getting fully utilised.