Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

unable to set dataset object name same as item id.

Hello Team,

 

as mentioned in above subject line,

I want to dataset to be created when i create an item, i have achieved this task by OOTB extensions.

But by default, datasets are taking the name in "item id /item revision id" format instead of "item id"

 for example in below example, when i am creating item, dataset with below name is coming..

where dataset object name is 000030/A

 

pdf1.PNG

 

this object name i need as of item id means only 000030

 

pdf2.PNG

 

Even we can change the display name from business objects constant. but its real object name will be same,

so instead of changing its only display name, we want its object name should in required format.

 

3 REPLIES 3

Re: unable to set dataset object name same as item id.

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Datasets can have a global naming pattern

DATASET_saveas_pattern=${ItemID}-${RevisionID}

Or they can have unique naming pattern based on type

 

TC_ugmaster_name_separator=/
UGMASTER_saveas_pattern=${ItemID}/${RevisionID}
UGPART_saveas_pattern=${ItemID}-${RevisionID}-${UserText}
UGALTREP_saveas_pattern=${ItemID}-${RevisionID}-${UserText}

Following the format <ds_type>_saveas_pattern.

 

Creating a default dataset when an Item is created requires IRDC (configured in BMIDE). Look it up in help which is pretty good.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: unable to set dataset object name same as item id.

Hello randy,

 

Thanks for your reply,

 

I tried with below preferences but still I'm unable to set the name as only item id.

 

can it be possible without writing code?

 

 

Re: unable to set dataset object name same as item id.

Experimenter
Experimenter

Hi Sir,

 

In IRDC you can have the name of dataset same as the $item_id.

In BMIDE create the required IRDC goto  IRDC Dataset Naming Page, in Source Dataset Naming Rule click Add.

Then select item_id in attribute for name from the drop down .

 

Hope this helps.

 

 

Regards,

Shashi