04-21-2018 12:04 PM - edited 04-22-2018 04:59 AM
I install the patch "Tc11.4.0_patch_3_wntx64" from base version 11.2
error message:
The following command returned a value of 1
"d:\Siemens\Teamcenter11\bin\preferences_manager" -u=infodba -pf=d:\Siemens\Teamcenter11\security\config1_infodba.pwf -g=dba -mode=delete -scope=SITE -preferences=TC_LAST_USED_PATTERNS
04-22-2018 01:28 AM - edited 04-22-2018 01:30 AM
Hi;
Please attach your log of installation(installdate-time_con guration-ID.log). it is under the root folder of application.
Thanks.
04-22-2018 05:03 AM
04-22-2018 07:49 AM - edited 04-22-2018 08:07 AM
Dear TerryWang;
Do below steps it may solve you issue.
1. remove jre installation from Programs and Features in Control Panel.(Jdk is all you need)
2. set variable JRE64_HOME=D:\Java\jdk1.8.0_151\jre
3. Set variabale JAVA_HOME=D:\Java\jdk1.8.0_151
4. set variable TCP_NODELAY=1 (if you haven't set)
Uninstall TC and try to reinstall again.
Please give your feedback here for others to use.
Thanks.
04-22-2018 08:26 AM
04-22-2018 08:31 AM
it is better to unistall it completely if possible.
04-22-2018 08:35 AM
If you did a complete unistallation when installing again install Base release and patch in one step.