Cancel
Showing results for 
Search instead for 
Did you mean: 

upgrade to nx10 - team center still opens old version

Creator
Creator

Howdy all, 

   I'm under the gun, (thinking it would be pretty straight forward) to upgrade from nx 8.5 to nx 10. We've got Teamcenter 10.1.4

On my test machine, i installed nx10, but cannot for the life of me get team center to open nx10 manager.  It keeps opening nx8.5 (or erroring after i uninstalled it)

 

I've futzed w/ every environment variable and config file i can find, 

changing from nx8~1.5 to C:\PROGRA~1\Siemens\NX10~1.0 

If i edit the start_nxmanager.bat to V28.0, that's great, the error message changes but still nothin'.

"Teamcenter integration for nx initialize failure 

nx cannot be starteed as teamcenter ingetration for nx(nx0tcin) database feature is not installed in teamcenter database."

 

I feel like i need to re-install everything, but I don't want to have to re-install teamcenter for all my users when it should just be a matter of pointing teamcenter at a different file.

 

Debugging has shown it is opening the ugs_router.exe in nx10\ugii\

 

I have been into several things, 

Maybe i cooked something else in the install on this machine?

 

6 REPLIES 6

Re: upgrade to nx10 - team center still opens old version

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

NX is using the file extension in Windows to determine where the ugs_router.exe is located. However, a little known fact is that the location of start_nxmanager.bat is actually stored in the registry. This can be difficult to debug when you have multiple clients running on the same machine.

 

I have a work around I like to use to set the registry key correctly depending on which client I'm launching. The hack will go into either portal\portal.bat or rac\otwportal.bat depending on your flavor of client (TEM vs OTW). Another hack in these same files is to ensure that FMS_HOME is set correctly and no previous FCC/TCCS is running from another environment.

 

What this does...

  • Sets FMS_HOME to the current client no matter what (remove if not defined).
  • Resets the registry key for the current location of start_nxmanager.bat
  • Stops any previously running FCC/TCCS (so that a new one can be started)

 

@echo off
rem 

setlocal

rem TPR is short for TC_PORTAL_ROOT to reduce command line length
title Teamcenter Rich Client

call "C:\Siemens\SDPROD\NXONLY\otw\otw_init.bat"

set TPR=C:\Siemens\SDPROD\NXONLY\rac
set FMS_HOME=C:\Siemens\SDPROD\NXONLY\tccs

rem use AUX_PATH env var for any additional required paths
rem save original path for external applications
set ORIGINAL_PATH=%PATH%
rem for optimal startup performance, keep the PATH length at a minimum
set PATH=%SYSTEMROOT%\system32;%FMS_HOME%\bin;%FMS_HOME%\lib;%TPR%;%AUX_PATH%

set JAVA_HOME=%TC_JRE_HOME%
set JRE_HOME=%TC_JRE_HOME%

%FMS_HOME%\bin\fccstat -stop
reg add HKCR\ugmportalfile\Shell\Open\command /d "%TPR%\start_nxmanager.bat" /f

:start_portal
cd /d %TPR%
set CLASSPATH=.;
set VM_XMX=512m

@echo Starting Teamcenter Rich Client...
start Teamcenter.exe %* -vm "%JRE_HOME%\bin\javaw.exe" -vmargs -Xmx%VM_XMX% -XX:MaxPermSize=128m -Xbootclasspath/a:"%JRE_HOME%\lib\plugin.jar";"%JRE_HOME%\lib\deploy.jar";"%JRE_HOME%\lib\javaws.jar"

The attached image highlights my edits.

 


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: upgrade to nx10 - team center still opens old version

Creator
Creator

Thnx for the quick resp.

While I work on this:

I do not seem to have an otw_init.bat on this machine. Thoughts?

 

J

 

 

Re: upgrade to nx10 - team center still opens old version

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Then you must have done a TEM installation. The code shown was for otwportal.bat. You'll need to modify portal.bat instead using the highlighted lines from the previosly attached image.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: upgrade to nx10 - team center still opens old version

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

BTW, the solution to your error is posted in an article by @CemAlpay titled "NX 10 integration to TC". Where your error was: "Teamcenter integration for nx initialize failure nx cannot be starteed as teamcenter ingetration for nx(nx0tcin) database feature is not installed in teamcenter database"

 

Is your Teamcenter version before Tc10.1.2? Then you might need the file mentioned by Cem.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: upgrade to nx10 - team center still opens old version

Creator
Creator

We're running 10.1.4

Re: upgrade to nx10 - team center still opens old version

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

- run tem.bat

- uncheck "NX Manager for Rich Client"

- let it complete

- exit tem

- run tem.bat

- check "NX Manager for Rich Client"

- make sure to point to the NX10.

- let it complete

- reapply 10.1.4 patch