Cancel
Showing results for 
Search instead for 
Did you mean: 

webtier - Service Server Manager do not start

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello Everyone,

 

I have installed Teamcenter 11.2 and after the web tier. I am able to input my login and password into the thin client, but I have the message that server manager service is not running, so I can not connect thin client.
I have already tried many solutions, but with no results.

Have someone ever had this situation?

 

 

Thanks!

4 REPLIES

Re: webtier - Service Server Manager do not start

Phenom
Phenom
Make sure you have (J2EE or .NET) Server Manager installed and Pool Manager is running either as Service or as command line.
if you launch TEM and navigate to "Features", the Server Manager feature is available under "Server Enhancements"

Re: webtier - Service Server Manager do not start

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I had the same problem as @Schmoller after my Tc11.2 install. SFB-Teamcenter-10054 fixed the .NET (RyuJIT) problem for me by applying the MS Hotfix rollup 3120239 (https://suppoort.microsoft.com/en-us/kb/3120239).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: webtier - Service Server Manager do not start

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

After the update 11.2.3, it worked!

 

1) Install TC 11.2

2) Install webtier (service server manager do not work)

3) Update TC 11.2.3 (service has started!)

 

Thanks!

Re: webtier - Service Server Manager do not start

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Yes, the fix was applied in Tc11.2.2 so patching to Tc11.2.3 would fix it.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4