Cancel
Showing results for 
Search instead for 
Did you mean: 

workflow condition task to condition task error

Pioneer
Pioneer

Hi Gurus,

 

I have a workflow with two condition task. The workflow is unable to continue after i select one of the task result that goes to Condition Task B. Please advise how i can resolve the following. There is no error message only showing pending.

Many thanks in advance.

 

 

Condition task B (Mulitple path that routes to others)

||

||

Condition Task A====> Perform Task 

 

Best Regards,

Steven

4 REPLIES 4

Re: workflow condition task to condition task error

Gears Phenom Gears Phenom
Gears Phenom

Hello, are you using other handlers for these tasks, other than EPM-check-condition?

 

Verify that Task B on the Start has an EPM-check-condition handler with the correct arguments:
-source_task=Task A
-decision={true | false |custom-result | ANY | error-code}

Re: workflow condition task to condition task error

Pioneer
Pioneer

Hi Arthur,

 

Many thanks for the reply.

No i am not using any other handler.

I have all the correct arguement for EPM-check-condition as mentioned by you.

 

 

 

 

Re: workflow condition task to condition task error

Gears Phenom Gears Phenom
Gears Phenom

This is strange. Try to create a process like me, will it work well for you? At me it works well.

 

My test process template:

wf1.png

 

When set "Custom result...", automatically creates EPM-check-condition with these arguments:

wf2.png

Re: workflow condition task to condition task error

Pioneer
Pioneer

Hi Arthur,

 

Many thanks for your help. It is solved.

 

Best Regards,

Steven