Cancel
Showing results for 
Search instead for 
Did you mean: 

What's New: Deployment Center 2.0

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

With the new Deployment Center, you can manage your Teamcenter PLM environment with ease. 

 

Easy, flexible and cost-effective product lifecycle management (PLM) tools for deployment are critical to help you realize the value of your investment. Deployment Center provides you with a centralized web-based application that you can use to deploy Teamcenter and manage your deployments. 

 

Deployment Center 2.0 was released in January 2018. This release is the next step in the Deployment Center's support for installing, patching and upgrading Teamcenter software easier, faster and with lower costs.

 

 

Deployment-Center-2.jpgTeamcenter has the PLM deployment tools for you.

Instructional Deployment Center Videos for Teamcenter Customers

 

To learn more about how to use Deployment Center 2.0 a set of instructional videos have been created. These videos demonstrate topics such as how to install the Deployment Center, register software, set up development, test and production type environments, create custom software in the BMIDE and deploy using the Deployment Center, using software versions and build version numbers to designate release numbers, how to install and update an environment with multiple software packages simultaneously. Since each video introduces concepts about the Deployment Center and subsequent videos build on these concepts, it is suggested that the videos be viewed in order for a cohesive learning experience.

 

Deployment Center 2.0 demonstration videos (customer-only access)

 

The following is a listing of the video titles:
1. Installation of the Deployment Center
2. Registering Software
3. Creating a single box development environment
4. Creating a distributed production environment
5. Installing Foundation and Active Workspace simultaneously
6. Importing pre-existing environments
7. Adding Active Workspace to a pre-existing environment
8. Editing Environments
9. Adding a Server Pool to an environment
10. Switching the FMS Master
11. Creating and deploying a new BMIDE Template software package
12. Importing and deploying a pre-existing BMIDE Template software package
13. Deploying software on the path to production
14. Using software versions
15. Using build versions for pre-release software
16. Using a composite software project
17. Automated software package generation
18. Simultaneously installing Foundation, Active Workspace, and custom software
19. Simultaneously updating Active Workspace and custom software

 

 

Comments
Solution Partner Phenom

The videos were a great help in understanding the scope and depth of Deployment Center. I now understand what the replacement is for compiling the tc.war file (J2EE Web Tier). I look forward to it also compiling the Login Service (ls.war) and Identity Service (id.war) for TcSSO. We will no longer need INSWEB at that point.

Community Manager

Thanks, Randy! 

Valued Contributor

Can we use DC for cloud environments yet?

Siemens Experimenter

The Deployment Center has a plan to support cloud type deployments. This will be something we will be looking to in the future.

Solution Partner Phenom

Deployment Center 2.0 does not check/add the "Log on as a Service" right for the assigned user (domain user in our case). Results in deploy.bat failure because the FSC service cannot be started (logon failure). Make sure you add the user to Local Security Policies > Local Policies > User Rights Assignment > Log on as a service before running deploy.bat.

Solution Partner Phenom

DC 2.0 does not set the system environment variable SPLM_LICENSE_SERVER so you'll need to do this manually before starting deploy.bat. Despite specifying the license server in DC, it is not honoring the value, and is defaulting to the local server. So if your license is running on a separate server the deployment fails.

Solution Partner Phenom

DC 2.0 doesn't appear ready for prime tiime yet. The deployment created E:\tmp\transientVolume, E:\usr\Siemens\tc_data, E:\usr\Siemens\volumes and E:\usr\Siemens\Teamcenter11\security\dcEnvName_infodba.pwf despite specifying that this was being deployed to wntx64 and not linux. My advice is to wait for the next release of DC before deploying Teamcenter. Probably fine if you want to deploy Active Workspace but I didn't get that far as you can tell. Going back to using TEM.

Siemens Experimenter

Thanks Randy for finding these, we will be working to get these taken care of in the next releases. For the last issue with the paths, I showed Randy yesterday that there is an "Advanced" paremeters toggle that shows you a list of additoinal properties for each component you are adding to your environment. By defalut the Deployment center shows you a shortened list of parameters. You can call that the "Quick Install" option. It shows you the least amount of steps to get the products installed. This is the default option.

 

To use the advanced option, when you get to the "Components" task in the process map, and then click on each component (ie. Corporate Server, FCS, RAC, Pool Server, etc) there is an icon (toggle) to the right of the component name. See the screenshot below. You can see the icon with 3 veritcal lines and a upward pointing chevron.

CS toggle.png

When you click this, the Deployment center will present the list of advanced options. This includes properties for paths, as mentioned by randy, as well as many other things like service names, etc.

If you look at these advanced settings you can see the values and alter them before you generate and deploy the scripts to your environment.

 

Hope this helps

Bob

Gears Phenom

I did get a distributed environment installed with Deployment Center. There are a few caveats as mentioned above. Also, it is best to use DC in Chrome and not IE. That seemed to resolve the wntx64 and linux path issues and updating correctly. It isn't perfect but when it works, much easier to deploy AW than manually. 

 

Jamie