Cancel
Showing results for 
Search instead for 
Did you mean: 

4-tier Richclient cannot connect, Schema problem

Builder
Builder

Hi.

I have an error "the schema file is out of date please regenerate" on richclient when connecting.

I've used to run command:

install -regen_schema_file [user props]

 

But the problem still exists. Is there any other command to publish or update schema after regeneration?

2 REPLIES 2

Re: 4-tier Richclient cannot connect, Schema problem

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You did not mention, but I believe the pool manager has been restarted after the regen?

 

Harish

Highlighted

Re: 4-tier Richclient cannot connect, Schema problem

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
You have to restart Server Manager after running the command. The command updates the TC_DATA\pom_schema_<db_server>_<db_instance> file. You should only run this command after stopping the environment and kicking out the users (clearlocks -assert_all_dead). When you restart then the error should be gone.
FYI, if you have more than one TC_DATA directory then you'll have to copy the pom_schema_xxx_xx file to the other TC_DATA directories. Note: If you don't know what I'm talking about then don't try it. All the TC_DATA directories must be from the same environment. Useful when multiple enterprise servers (running server manager) are involved.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4