Cancel
Showing results for 
Search instead for 
Did you mean: 

Access existing NX / Custom attributes from a SOA Client / Business Modeler

Experimenter
Experimenter

Hey,

 

we some CAD Models (NX) in our project. In NX, these have (calculated) properties like mass, volume and other attributes.

1 ) Is there a way to access these directly from within Teamcenter via the SOA Client bindings? Is there a similar way?

In Teamcenter, these are of type UGMASTER. I can't see any fields / methods related to CAD in anyway on this type, but NX somehow needs to store these files.

2) How does NX associate its CAD files with the Object? If Teamcenter has no direct Information about the attributes, we'd like to at least access them via an NX SDK or something.

 

And secondly, if we'd want to store custom attributes on these items, we'd probably have to create templates in business modeler, right?

 

Many thanks in advance!

1 REPLY

Re: Access existing NX / Custom attributes from a SOA Client / Business Modeler

Experimenter
Experimenter

The feature i was looking for is "Named References"