Cancel
Showing results for 
Search instead for 
Did you mean: 

Active Integrations or data sharing options

Experimenter
Experimenter

Hello Experts,

 

Is there some overview of what are the current options available in Teamcenter regarding Data Sharing. Lets say if I want to share BOM information (on regular interval) from independent third party system to Teamcenter, then what tools could I use with monitoring capablities ??

 

As I understood some of the tools are TcIF and T4EA. So where could I find the capabilities and comparision information ?

 

Thanks in advance!

 

Best Regards

Awadhesh

4 REPLIES 4

Re: Active Integrations or data sharing options

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
There was a good presentation at Siemens PLM Connection 2018 this year on how to decide between TcIF and T4EA. Basically it comes down to if you need to share CAD data. T4EA does not so for your use-case you can use either one. Your use-case is integration more than data sharing which eliminates a few of the options. Of the two, T4EA is easier to implement in my opinion but there are examples for TcIF (see Supplier Integration).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Active Integrations or data sharing options

Experimenter
Experimenter
Hello Randy,
Thanks for the information. your comment was very helpful.
I do not have the member logic currently. If the document is public, could you please share the link.

Best Regards,
Awadhesh

Re: Active Integrations or data sharing options

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

The presentation does not say it is restricted. See attached.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Active Integrations or data sharing options

Experimenter
Experimenter

Thanks Very much Randy !