Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly Load Failure

Valued Contributor
Valued Contributor

When opening an assembly in teamcener I get the error:

"Could not open XXXXXXX/XXXX.

The following files could not be loaded, causing this open to fail:

XXXXXXX/XXXX - Incorrect object for this operation." 

 

This only occurs with the same two assemblies.  The first one will open normally, then try to open the second one, I receive the error stated above.

 

Can anybody help with this?

 

Thanks

Jake
1 REPLY 1

Re: Assembly Load Failure

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
I would suggest calling the GTAC 'Teamcenter Integration for NX' support group.

Regards, Ben