Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly

Genius
Genius

Hi guys.

 

I want to do an assembly with parts from teamcenter.

When I want to create an assembly I am always asked to save before I start building the assembly.

 

Is it possible to create an assembly without having to save it to teamcenter?

1 REPLY

Re: Assembly

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Dazzie,

 

If you are creating new Assembly Structure in NXManager i.e. Teamcenter integrated NX, then it is not possible to create an assembly without saving it, whereas you can use existing assembly for the same purpose.

 

Either you can export the data outside teamcenter and create a assembly in NativeNX,

Or you can create a dummy Item in teamcenter which can be used for trail and error purpose.

 

I guess you might have the idea of above given details, however customizing the link between TC and NX for particular temporary purpose will be disastrous and also it is not recommended.