Cancel
Showing results for 
Search instead for 
Did you mean: 

Attach pdf file to a Change Notice

Hi, I'm user of TeamCenter from 1 year.

I need to attach an internal file (pdf/image/etc) to a Change Notice Revision.

 

How can I attach it? 

 

15 REPLIES

Re: Attach pdf file to a Change Notice

Phenom
Phenom

Good Afternoon, create and place the necessary dataset in a pseudo folder Reference Items 

Re: Attach pdf file to a Change Notice

How and where can I create this pseudo folder?

 

My Change Notice has the following folder:

-Change report Information

-Problem Items

-Solution Items

-Implements

-Implemented by

 

I cannot add new folder in Change Notice Revision

Re: Attach pdf file to a Change Notice

Phenom
Phenom

What version of the Teamcenter do you use? In Teamsenter 10 it was called, as I wrote to you earlier. In your case, it is most likely called Change report Information.

Re: Attach pdf file to a Change Notice

I'm using TeamCenter 11

I can attach a pdf file into the folder Change Report Information but when I start the workflow to release the change it is overwritten with the deafault pdf called Change Notice Report_...

 

How can I do to avoid the overwrite of the file?

Re: Attach pdf file to a Change Notice

Phenom
Phenom

Check relation type on your attach pdf file in pseudo folder Change report Information is that a same type like on last image?

 

check relation.png

 

check relation1.png

 

 

Re: Attach pdf file to a Change Notice

I have not this field or similar. The picture show my option.

 

Immagine.jpg

 

Re: Attach pdf file to a Change Notice

Phenom
Phenom

When you click right button mouse, you stand on pdf dataset in pseudo folder Change report Information?

Re: Attach pdf file to a Change Notice

Yes, the upper pic is the result of right click on the pdf into the pseudo folder Change Report Information.

To attach that file I've used File/New/Dataset and selected the pdf.

Re: Attach pdf file to a Change Notice

Phenom
Phenom

Try use Edit menu

 

Edit menu.png