Cancel
Showing results for 
Search instead for 
Did you mean: 

BOM LINE PROP

Pioneer
Pioneer

Hi experts,

 

In teamcenter structure manager there is bom line property called bounding box, I heard that the value for this bounding box is fetched from , setting somethings in NX.

Can any one tell me , what i have to do in NX to get bounding box value in structure manager of teamcenter.

 

Thanks. 

8 REPLIES

Re: BOM LINE PROP

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @girish,

 

Have you installed the "Bounding box generation from NX" Engineering Process Management Extension in TEM?  If you have, that should be enough to get bounding box information displayed in the Bounded Boxes column of Structure Manager.

 

Regards, Ben

Re: BOM LINE PROP

Hi @BenBroad,

Under named references of the UGMASTER dataset, I can see the 'UGPART-BBOX' form. When opened, it shows the respective values xmax,xmin etc.bb.PNG

When same item sent to the Structure Manager, There is nothing displayed under the column 'Bounding Boxes'. Is it needed to set any additional preferences for the same?

 

Also, irrespective of the unit of part in NX whether it is Metric or Inch. Values under UGPART-BBOX are displayed in 'Meters'. I have already referred the documentation link Structure Update Forms. Is there any way, if I have created NX part using Inch unit so that values in BBOX form should also be displayed with the same unit.

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: BOM LINE PROP

Pioneer
Pioneer
Hi BenBroad,
Thanks for response. I thought that bbox value is necessary to get proximity value box in design context module of TC.
But still i am not getting proximity box in design context.
Please let me know is there any prerequisites i need to set before using design context.

Regards
giri

Re: BOM LINE PROP

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Ganesh_Kadole,

 

Refer to the question that I posed to Girish.  Originally I was getting the same results as you and I found that I did not have "Bounding box generation from NX" installed in TEM.  Once installed the values were seen in the Bounding Boxes column.  No other preferences were changed in NX or TC.  In fact, I was originally turning on "Save True Shape" in the NX Save Options, but did not enable it in my final test to get the values to display in SM.

 

Regards, Ben

Re: BOM LINE PROP

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @girish,

 

Are you working on imported NX data or are you creating new NX data?  Do your UGMASTER datasets contain bounding box (UGPART-BBOX) Named References?  If you imported the assemblies you'll have to generate the bounding box values in Teamcenter.

 

Regards, Ben

Re: BOM LINE PROP

Pioneer
Pioneer
Yes ben,

I am only creating NX data , and am getting bounding box value also.
But question is about design context. Still proximity value box in design context module is not getting appeared.

Regards
Giri

Re: BOM LINE PROP

Siemens Phenom Siemens Phenom
Siemens Phenom

I wonder if you need to generate true shape data as well?  Unfortunately I'm not familiar with the Design Context module.  Hopefully someone else will be able to answer your question, or you could try calling GTAC Teamcenter Application Support.

 

Regards, Ben

Re: BOM LINE PROP

Thank you @BenBroad for the validation, I will check that! Smiley Happy

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2