Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot Connect to or start the application UG/Manager V22.0

Pioneer
Pioneer

Dear Friends

 

i installed teamcenter 8.3.1 and nx 8.5 with rich client otw.

now i open teamcenter, and selected standard_therad_metric model and try open NX. and show me error:

Cannot Connect to or start the application UG/Manager V22.0

please tell me how to do it?

 

thanks

3 REPLIES

Re: Cannot Connect to or start the application UG/Manager V22.0

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

Answered your post in the Teamcenter Admin Forum. INSWEB, NX version incorrect (V22.0 is NX4). You want V26.5 for NX 8.5.

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Cannot Connect to or start the application UG/Manager V22.0

Pioneer
Pioneer

Dear Randy

 

 

i change v22.0 to v26.5 insweb and open nx now,

but now after open nx show me error:

An internal error occured in the Teamcenter SOA client

Error number:940228

please tell me how to do it?

 

thanks

 

Re: Cannot Connect to or start the application UG/Manager V22.0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you don't cross-post, you make it much easier for us to help you.

 

Further discussion of this topic should be carried out at the Tc admin forum.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide