Cancel
Showing results for 
Search instead for 
Did you mean: 

Change TcServer Character Encoding Settings manually

Genius
Genius

Hello;

I want to change/check "TcServer Character Encoding Settings" after installing client. Is there anyway to do that?

when I use RapidStart then PreConfigured installation choice, there is no step to change this setting in installation.

 

I really appreciate your hepls.

Best Regards.

7 REPLIES 7

Re: Change TcServer Character Encoding Settings manually

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Uninstall and reinstalling the client is the easiest way to correct it.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Change TcServer Character Encoding Settings manually

Siemens Creator Siemens Creator
Siemens Creator

Hi,

 

You can't modify tc character encoding but you can check.

In TC_DATA, you can see tc_profilevars.bat.

The environment value of TC_XML_ENCODING in bat file is your currently charaset.

I guess this setting is defined by DB charaset automatically. 

 

Best Regards,

Re: Change TcServer Character Encoding Settings manually

Genius
Genius

Hi;

Thanks for your reply. But this setting doesn't change the encoding. I test it and it didn't work. thanks anyway.

Re: Change TcServer Character Encoding Settings manually

Genius
Genius

Hi;

I think it is the only way after trying alot.

 

thanks.

Re: Change TcServer Character Encoding Settings manually

Experimenter
Experimenter

Hi,

 

Is there a way to change the TC server character encoding. We have selected a wrong encoding during installatio and want to revert to the right one. Tried different steps but its not helping.

Highlighted

Re: Change TcServer Character Encoding Settings manually

Genius
Genius

@tengapra

What character set do you want to use?

change TC_DATA\tc_profilevars

Set TC_XML_ENCODING parameter to your desied one.

also

2-Tier Client:

In the TC_ROOT/iiopservers/Start_TcServer1set TC_CHARACTER_ENCODING_SET to your desied.

4-Tier Client:

In the TC_ROOT/pool_manager/mgrstartMYDB,set TC_CHARACTER_ENCODING_SET to your desied.

 

BR.

Re: Change TcServer Character Encoding Settings manually

Experimenter
Experimenter

Thank you., We use UTF-8 and we wanted to chage to ISO-18559-1

We amde the below changes but still the syslog was pointing to UTF-8.

 

After we set the LANG env variable to en_US, then the TcServer Character Encoding was displayed correctly as ISO-18559-1