Cancel
Showing results for 
Search instead for 
Did you mean: 

Change Unit of measure - TC 10.1.0.1

Pioneer
Pioneer

Hello everyone

 

Is there a way to change the UOM of an Item used in multiple assemblies without removing this Item from those assemblies?

We are trying to standardize units accross our differents platform and this task is becoming a nightmare.

 

We are using TC 10.1.0.1 with NX 8.5.3.

 

Laurenj.

 

Unit of measure.png

4 REPLIES

Re: Change Unit of measure - TC 10.1.0.1

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can batch change using SQL however it is dangerous so I won't post the solution in this forum. You'll have to contact me directly. rellsworth at sherpa-design.com

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Change Unit of measure - TC 10.1.0.1

Pioneer
Pioneer
Thanks for the quick answer! I sent you a mail a moment ago.

Laurenj.

Re: Change Unit of measure - TC 10.1.0.1

Experimenter
Experimenter

Hello,

We have similar issue for a item which is a assembly.

Please suggest.

Re: Change Unit of measure - TC 10.1.0.1

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thanks to Rick Horwart who wrote the attached ITK. As you may know, ITK doesn't bypass the application layer like direct SQL so its inherently safer to use (and supported). Not all ITK is equal but Rick did a great job. He even compiled it on Tc10.1.0 to validate no errors before sending. You'll need to compile the attached into an external program to be used on the Teamcenter command line. Enjoy!


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4