Cancel
Showing results for 
Search instead for 
Did you mean: 

Classification Admin UI in NX

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

Is it possible to bring Classification Admin UI in NX Client

if yes , how to configure to view it in NX Client

 

Regards

Vamsi Krishna

6 REPLIES

Re: Classification Admin UI in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

Not entire Classification Admin UI but 'Classification Root' folder can be accessed from NX.

 

Start NX from TC, In 'Reuse Library' navigator you can see the Classification Root folder.

 

classi.PNG

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Classification Admin UI in NX

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Another possibility is BCT aClass which is designed to show Classification in NX (or Solid edge).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Classification Admin UI in NX

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @hcl,

What are you looking to accomplish?

If you're simply looking to classify individual parts in NX this can be done, with the part open in the session, by right clicking the node (class) in the Reuse Library under the "Classification Root" folder and choosing "Classify Part".  You'll be presented with the following dialog allowing you to match predefined classification attributes with values in the part:

Screenshot - 4_4_2017 , 8_41_02 AM.png

 

Regards, Ben

Re: Classification Admin UI in NX

Legend
Legend

There was question - is it possible to have Classification Admin functionality from NX?

 

The answer - NO

 

In NX you can only have access to classification root for search or classify/

note: nx_access_tcclass license required for that

 

 

 

Re: Classification Admin UI in NX

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

@alex_c, I understand the question, but you have to also question why it is necessary to see the UI in NX. Is the requirement to see the entire Classification Admin UI in NX, or would one small part suffice? One has to make certain assumptions when such an ambiguous question is asked, one of which in this case could be that the only requirement is just to classify parts - in which case, yes, this can be done in NX. Admittedly no one answered the question, which is 'no', the entire Classification Admin UI cannot be viewed in NX. That said, @hcl, may I ask why you need to see it in NX?

 

Regards, Ben

Re: Classification Admin UI in NX

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks Ben for your response