Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Configure multiple Master FSC

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

I am looking for a failover FSC configuration.

Setup:

I have one server (say server1), on which I have installed Coorporate server, volume, FSC, pool manager & JBOSS. I am able to access it from a 4-tier client without any issue.

 

Now I wan to create a configuration, where if my FSC on server1 is down, client should be able to connect with another FSC.  (Remember, this is also the MASTER FSC)

For this I have installed FSC on server2. I have updated FMS_bootstrap_url preference, also fcc.xml on client macine.

What Else I need to do so that client can work with server2 FSC if server1 FSC is down.

Please note I have only one volume located on server1.

 

Regards,

Piyush Garg