Cancel
Showing results for 
Search instead for 
Did you mean: 

Confirmation Pop-up Boxes for Check-in / Check-out

Experimenter
Experimenter

HI,

 

Can someone please tell how to turn the confirmation pop-up box off. It's driving me nuts having to confirm on every check-in / check-out I do. I do heaps and it becomes too much everyday.

 

Cheers

Bas

11 REPLIES

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Genius
Genius

When you check-out / Check-in, Click on the small check box " Do not show this again". That should do it.

Teamcenter 10.1.3
TC Visualization 10.1.3 (Custom Patch)
NX:8.5 | NX 9.02 | Catia V5 R2012 | AutoCAD 2015 | In-Context Editor |

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Try these,

  • Confirm_cancel_checkout_suppressed = true
  • Confirm_checkin_suppressed = true
  • Confirm_checkout_suppressed = true

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Pioneer
Pioneer

Yes ... and if you are using the Client4Office as well you might notice that if suppressing the popup in RAC it wil make it appear in Office and vise versa.

 

Please report / add yourself to PR 7477139 "confirm_checkout_suppressed inconsistency between Office Clien and Rich Client."

Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP4 + TC10.1.7.1
Testing: NX11.0.2.7 MP4 + TC10.1.7.1
Development: C#

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Experimenter
Experimenter

Hi...i'm using 10.1.4. I don't get a checkbox that would allow me to easily do this.

Thanks anyway

 

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Experimenter
Experimenter
Hi Randy,
Would this apply it to all users or can it be applied to a certain group?

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Those are Site preferences in my installations.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Experimenter
Experimenter

Came across this today and wanted to add for anyone else who has this question.

There is a preference for controlling the visiblity of the checkbox which is set to false by default. From the documentation for 10.1.6:

Preference = Confirmation_shown_on_reservation_dialogs

DESCRIPTION
Specifies whether a Don’t show confirmation dialog again check box is displayed in the Check-Out , Cancel Check-Out , and Check-In dialog boxes in the rich client and thin client.

VALID VALUES
true = The Don’t show confirmation dialog again check box is displayed.
false = The Don’t show confirmation dialog again check box is not displayed.

DEFAULT VALUES
false
DEFAULT PROTECTION SCOPE
Site preference.

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Genius
Genius
TylerB

This is good in RAC. when we open any part in Solid edge. Does not ask"do you you want checkout"?. it checkout automatically, Is it possible to ask us to decide?

Re: Confirmation Pop-up Boxes for Check-in / Check-out

Experimenter
Experimenter

Venny - We don't use Solid Edge here so I don't have any experience with that setup.  The preferences referenced above by Randy can specify the state for the check box (true/false).   Maybe there is a similar setting that is available in Solid Edge?