Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating BOM or assembly in Teamcenter 11

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

How can I create an assembly with empty Items in Teamcenter without NX?

Is it possible in Structure Manager?

 

Cem

3 REPLIES

Re: Creating BOM or assembly in Teamcenter 11

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Yes, you can build your assembly in Structure Manager then send it to NX.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Creating BOM or assembly in Teamcenter 11

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
you can do this in 2 ways:

1. Copy/Paste: Select an Item/ItemRevision and copy. Then open Structure Manager and paste. If you select an item1 in structure manager and paste item2, then item2 will be child of item1.

2. Create Items: Open structure manager and create item using File-New-Item. If item1 is selected while creating item2, item1 will be the parent of item2

Save the changes in the end.

Re: Creating BOM or assembly in Teamcenter 11

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

 

If you donot have NX installed then also you can also create a Assembly structure in Teamcenter

 

Create a new Item -  File > New > Item > Assign ID and Rev > Finish.

and then select the Newly created Item Revision  -

and Add the BVR by  - File > New > BOM View Revision > Ok

You can also add BVR to existing item revison, Once BVR is added to the Item revisoin then it is open the Item in Structure manager and add number of component you want to add to it as mentioned by Amol_XPLM.

 

Please find attachment for details.

If you donot have the option as described in Image, contact your IT support.