Cancel
Showing results for 
Search instead for 
Did you mean: 

Creation of linked data resources in the RAC

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

I'm working with the polarion integration on teamcenter, mostly on active workspace. So I add to install linked data framework

 

I wanted to kow how I could create a linked data framework resource in the RAC ?

 

Thnak you in advance,

 

Sènan

 

 

4 REPLIES

Re: Creation of linked data resources in the RAC

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The Rich Application Client (RAC) is not the same as Active Workspace. Also, LDF is for "displaying" data from external systems (read only). I think you want TcIF (Teamcenter Integration Framework) for Polarion? See platform_extensibility_config.pdf.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Creation of linked data resources in the RAC

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

If displaying data from Polarion is what I want to create, does it also have to be with TcIF ?

Re: Creation of linked data resources in the RAC

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
I guess it depends on your use-case. LDF will show read-only data (one-way). If that's your goal instead of interacting with the Polarion data in Teamcenter then you're on the right track. My assumption is that you want a fuller integration where you can interact with it (two-way).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Creation of linked data resources in the RAC

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
I'm not specially looking for the fuller integration as the read-only functioning is fine for me on Active Workspace so it will be thesame for me on the RAC.