Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom OTW install for Creo

Experimenter
Experimenter

Hi All,

I am trying configure CERO OTW integration TC11.3. I have checked in GTAC solutions ,
OTW for CREO is not available as it is available for CATIA (Teamcenter_Integration_for_CATIAV5_11.0.4.3_tc11.2_OTW.zip)

Kindly help me with your valuable suggestions for building custom icd(OTW) for CREO integration.

 

 

Best Regards

Ravikumar

1 REPLY

Re: Custom OTW install for Creo

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
The Creo (IPEM) and SolidWorks (SWIM) integrations are built by the same third party so they behave similarly. It does not behave like the Catia integration (TCIC). The integration is an executable for which you will select "Client" to install the software on the client. "Server" for installing data types, prefs, etc on the server. You will also need to install the JT translator for Creo on the client. Install order I usually follow is:
1. Install JRE x64 and x86 versions.
2. Creo - make sure to install application feature "API Toolkits" > "Creo Object TOOLKIT Java and JLink"
3. JT Translator for Creo
4. OTW Teamcenter
5. Teamcenter Integration for Creo (IPEM) - like SWIM, IPEM can be installed silently using "ipemsetup.exe -f ipemsetup.properties".

Naturally, I've scripted the client install to prevent errors and omissions.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4