Cancel
Showing results for 
Search instead for 
Did you mean: 

Does Teamcenter run under Windows 8?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Does Teamcenter run under Windows 8?

8 REPLIES 8

Re: Does Teamcenter run under Windows 8?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Tc10.1 supports Win 8 Pro (client only) and Tc10.1.3 supports Win 8.1.

https://support.industrysoftware.automation.siemens.com/certification/teamcenter.shtml

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Does Teamcenter run under Windows 8?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Is TeamCenter 10.1.2 compatible with Windows 8?

Re: Does Teamcenter run under Windows 8?

Pioneer
Pioneer

Mr. Banzai

 

Our User consumer using win 8 OS, Teamcenter 10.1.2 for OS win8 notyet upgrade to 8.1 and still running on TC 10.1.2

 

Thanks

Sudikin

TC10.1.2

NX10

SW2015

Re: Does Teamcenter run under Windows 8?

Experimenter
Experimenter

Randy,

Does Tc10.1.4 support Windows 10?

Thanks,

 

Thach

Re: Does Teamcenter run under Windows 8?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Windows 10 isn't officially supported until Tc10.1.6. You'll also want to read SFB-Teamcenter-10005 to be clear on Win10 patching.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Does Teamcenter run under Windows 8?

Pioneer
Pioneer

Mr. Randy

Thanks for your information, but now we use TC10.1.2 running on windows 10.

Re: Does Teamcenter run under Windows 8?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TCSRP1 wrote:

Mr. Randy

Thanks for your information, but now we use TC10.1.2 running on windows 10.


The problem, is that you run an unsupported configuration, so if the problem you encounter cannot be duplicated with a supported configuration, you won't get a fix and you are told to upgrade to the supported configuration.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Does Teamcenter run under Windows 8?

Pioneer
Pioneer

Mr. Stefan

You are right, because in our company have upgraded all windows pc without exception. and this my be at risk of running applications. hopefully no serious problems.

 

Thank You