Cancel
Showing results for 
Search instead for 
Did you mean: 

Error= FCC start script is missing or inaccessible. FMS_HOME may be incorrect.

Genius
Genius

Hello

This happened suddenly:

Error= FCC start script is missing or inaccessible. FMS_HOME may be incorrect.

NX11.0.2.7

sdsddjpg.jpg

11 REPLIES 11

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Genius
Genius

Waited 1 day and TC11 still won't allow me to log-in.

  • Here are the enviroment variables. ( No FMS HOME.)

Someone said this would help ? I have no idea.

Deleted data from: ( This is easy and it's ok but won't do anything.)

  • C:\Users\\FCCCache
  • C:\Users\\Siemens\logs
  • C:\Users\\Teamcenter\RAC
  • C:\Users\\Appdata \Local\Temp

Start FMS-service ? ( I don't know where FMS HOME is located ? )

  1. cd %FMS_HOME%
  2. cd bin
  3. fccstat –status
  4. fccstat –kill
  5. fccstat –start

Manually start it with "Admin-rights" ? ( I don't know the Admin's user+pass ? )

  • http://host:8083/mgmt/console ( *host*=Teamcenter server name.)
 
 

Untit313ddled.jpg

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, do you have installed 2 Tier or 4 Tier Teamcenter client? Do you use only one Teamcenter client? If you use one Teamcenter client, usually
FMS_HOME is set in the environment variables of the computer. I don't see it on your screenshot.

 

Example environment variable:
FMS_HOME=<client_path>\tccs

where <client_path> path to the installed client

Highlighted

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Genius
Genius

TCPROD 4-tier

  • I log in to 4-tier.

1 Teamcenter client ?

  • I don't know. We have multiple users=usernames.
  • No "FMS_HOME=<client_path>\tccs"
  • I have added manually: UGII_ENV_FILE    \\PRO-TC-001\NX_Site\ugii_env.dat

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Legend
Legend

FMS_HOME is normally set in portal.bat (%TC_ROOT%\portal\portal.bat)

you should have lines like

set TPR=C:\PLM\TC113\portal
if not defined FMS_HOME set FMS_HOME=C:\PLM\TC113\tccs

 

Did you pin your Teamcenter to the Taskbar in Windows?

then it will not work, because portal.bat is not pinned, Windows will pin 'Teamcenter.exe', not the batch file

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Genius
Genius
set TPR=C:\Siemens\TCPROD\TC114T\portal
set FMS_HOME=C:\Siemens\TCPROD\TC114T\tccs
%FMS_HOME%\bin\fccstat -kill

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Legend
Legend

That looks ok,

fccstat -kill is not necessarily needed

 

can you comment this out

rem %FMS_HOME%\bin\fccstat -kill

 

and try again to start portal.bat

 

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Genius
Genius

There were never FMS_HOME in Environment variables and it still worked for many years.

  • Why FMS_HOME is important ?

Untitl1212ed.jpg

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Legend
Legend

Re: Error= FCC start script is missing or inaccessible. FMS HOME may be incorrect.

Genius
Genius

How to set FMS_HOME environment variable again ?
High change that my virus scanner has deleted it accidentally.