Cancel
Showing results for 
Search instead for 
Did you mean: 

Error on save after revise.

Creator
Creator

Hello again.

 

I've revised some items and after that I'm opening them in NX to work on them.

 

One of this items don't let me save it showing below message:


ERROR-NX9034_previous_version_not_loaded.png




 

Checking in TCe named references I noticed that it probably made something wrong when I revised it.

 

As you can see in below image it is calling the 00 revision ugpart-atributes file in 01 revision.


ERROR-NX9034_attribute_not_leveled_up.png












 

Something I can do to correct it or I need to delete this revision and create it again?

Thanks.

 

3 REPLIES

Re: Error on save after revise.

Phenom
Phenom

It looks like it still refers the dataset from old revision. Because when you revise, by default the Deep Copy Rule on datasets is 'Copy As Reference'. I don't know if this can now be corrected (as per my knowledge, deleting the revision is the only option); but while revising next time you could use Deep Copy rule 'Copy As Object'. OR: depending upon the processes/requirements in your environment, change the Deep Copy Rule to 'Copy As Object' for these type of datasets using BMIDE.

Re: Error on save after revise.

Creator
Creator

Thanks for reply, splm2005.

 

The "BMIDE" and "Deep copy rule" options sounds like more advanced knowledge and permissions that I have now.

 

I'll keep the deleting and re-create option for now.

Re: Error on save after revise.

Experimenter
Experimenter

Hello!

 Although changed the Deep Copy Rule to 'Copy As Object' for these type of datasets using BMIDE, I have similar question:

Creo Design tool, After revised in Teamcenter; The naming reference of ItemRevision ID "B" is same to  the naming reference of "A"; I open object file of the revision "B"  through the TC&Creo integration;but the error issue:

Creo integration Error.pngBMIDE Deep copy rule.pngitemrevision  revised.png

 

The right pictures is error image、deep copy rule、item revise in sequence.

 

Give me some suggestions to correct it!

 

Thanks in advance!